Avnet Electronics Marketing - Community Forum
    |   
 
Home Design Services My Account About Avnet
Reply
Avnet Employee
dsp_support
Posts: 14
Registered: ‎09-28-2009
0

Welcome to the Avnet 'FPGA-based System Design with High-Speed Data Converters' forum

Welcome to the Avnet 'FPGA-based System Design with High-Speed Data Converters' forum. This site is dedicated exclusively to Xilinx FPGA-based data acquisition among workshop attendees. Presently, it is not open to the general Avnet customer base.

 

Right now we are finalizing the last updates to the lab instructions and reference designs to provide the highest-quality design tutorials. We plan to post the material on the Avnet server this week, at which time we will notify you by e-mail and through this forum.

 

Stay tuned for instructions to download the workshop material from the Avnet server later this week.

 

regards,

 

Luc Langlois

Global technical Marketing, DSP
Avnet

New Member
pal_sandip
Posts: 2
Registered: ‎08-19-2010
0

Re: Welcome to the Avnet 'FPGA-based System Design with High-Speed Data Converters' forum

Please send the details of support materials available on the above subject.

 

E-mail: pal_sandip_cal@yahoo.com

New Member
AstroBoy
Posts: 1
Registered: ‎07-24-2011
0

Re: Welcome to the Avnet 'FPGA-based System Design with High-Speed Data Converters' forum

Hi Luc

 

I attended your 'FPGA-based System Design with High-Speed Data Converters' course in Singapore during the last March. Currently, I am implementing the same interface design using IODelays & ISERDES primitives running at 500Mbit/s with a deserialization factor of 4 in Virtex 5. I have performed post-layout simulation using ModelSim 6.3e and looked into the input clock & data signals to all the ISERDES. I realized the input clock edge is not aligned to the center of the data eye. I was wondering if I should adjust the phase of the clock using the PLL such that it is aligned at the center of the data eye. Please advise. Hope to hear from you soon. Thanks.

Visitor
wqiang_max
Posts: 1
Registered: ‎02-15-2012
0

Re: Welcome to the Avnet 'FPGA-based System Design with High-Speed Data Converters' forum

Could someone be kind to share me the course material? I am going to start some similar design with FPGA based platform.

 

my email:wqiang_max@hotmail.com