Avnet Electronics Marketing - Community Forum
    |   
 
Home Design Services My Account About Avnet
Reply
Contributor
floke
Posts: 19
Registered: ‎11-25-2010
0
Accepted Solution

Mini Module Plus complete pinning

Is there a file (e.g. ucf ) with the complete mapping from FPGA pin to JX1 and JX2 connector pins for the Virtex5 FX 30T mini module plus board. The xbd-files covers some but not all of the available IOs.

A  schematic netlist would be helpful too.

Avnet Employee
npoureh
Posts: 339
Registered: ‎05-05-2009

Re: Mini Module Plus complete pinning

Here you go. The attached zip file contains two UCF, one for each MMP slot on the MMP baseboard.

Contributor
floke
Posts: 19
Registered: ‎11-25-2010
0

Re: Mini Module Plus complete pinning

Thanks,

Do you also have a file with connection between JXz_SE_IO_xy and JXz_DIFF_IO_xy and pin number of Samtec conector?

A netlist instead of pdf file for the MMP schemtic would be helpful.

Avnet Employee
KountryK
Posts: 46
Registered: ‎07-09-2009
0

Re: Mini Module Plus complete pinning

Avnet provides our customers pdfs of schematics, mechanicals, layout and BOMs on our Design Resourcse Center.

https://www.em.avnet.com/en-us/design/drc/pages/supportanddownloads.aspx?RelatedId=220

 

In regards to the source for these design files, we make our engineering and fabrication files available to Avnet customers free of charge upon request. The files are not posted to external sites because we want to make sure customers always get the most up to date files and need to track who is receiving them. For this reason we do not distribute the files beyond the intended customer.

 

In addition to gerber files we can also offer the native design files. Older projects were developed using Orcad for schematic capture and PADS for layout but we have been using Altium both over the last 3 years.

 

To request files, we ask that you supply the following information:

1. customer name and address.

2. company name and address

3. project name for files usage.

4. description of application

5. intended use of the files

6. format customer wishes to receive the files in (Native, ASCI, Gerber, PDF).

8. Local Avnet FAE and AM.

 

 

If you find these files and/or our kits valuable, testimonials are welcomed and encouraged.

 

You may not want to share this information I've requested through the forum.  Thus you can open a case with Avnet Centralized Technical Support Centralized-Support@avnet.com to request these files.

 

B/r,

Russ

Contributor
floke
Posts: 19
Registered: ‎11-25-2010
0

Re: Mini Module Plus complete pinning

Thanks,

By now I have mapped all my pins but thumbs up for providing this service.

BR Jonas