- Subscribe to RSS Feed
- Mark Topic as New
- Mark Topic as Read
- Float this Topic to the Top
- Bookmark
- Subscribe
- Printer Friendly Page
Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 03:38 AM
Hi Mario
I tried to port a PLB-based IVK design (a slight modification of Camera Frame Buffer demo) from ISE 13.1 to 13.3. I could generate the bitstream in XPS 13.3 and the SW in SDK 13.3. However, on the IVK target the SW hangs in routine fmc_iic_xps_IicRead at line
} while (StatusReg != (XIIC_SR_RX_FIFO_EMPTY_MASK ....
So it looks as there is something wrong with the IIC access to the FMC module.
Can you give me a hint on what the problem could be? Is it related to the newer versions of EDK IP blocks available in 13.3?
Regards,
Juergen
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 05:51 AM
Juergen,
This could be related to driver updates.
In order to test this, comment out the "FMC Validation" code, but keep the call to fmc_ipmi_enable( ) ...
#if 0
// FMC Module Validation
if ( fmc_ipmi_detect( &fmc_ipmi_iic, "FMC-IMAGEOV", FMC_ID_SLOT1 ) )
{
fmc_ipmi_enable( &fmc_ipmi_iic, FMC_ID_SLOT1 );
}
else
{
fmc_ipmi_disable( &fmc_ipmi_iic, FMC_ID_SLOT1 );
exit(0);
}
#else
// Skip FMC Module Validation
xil_printf("Skipping FMC Module Validation ...\r\n" );
fmc_ipmi_enable( &fmc_ipmi_iic, FMC_ID_SLOT1 );
#endif
Let me know if your design works with this modification.
Regards,
Mario.
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 06:24 AM
Mario,
Yes, it works!
I saw that there was a driver update for the xps_iic module between 13.1 and 13.3. I think it must be related to this, since xps_iic is the only module involved that had an update.
Although I dont understand exactly why fpGpoRead still works with 13.3 and fpIicRead doesn't, I appreaciate your fast support very much.
Thanks a lot,
Juergen
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 06:33 AM
Juergen,
Would you be willing to share your 13.4 project for the benefit of the community ?
I will not be updating the PLB-based designs.
Instead, I will be moving to AXI-based designs.
Regards,
Mario.
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 06:56 AM
Sure, I will be happy to share.
The design is part of a real-time video processing lab I am currently preparing here at Lucerne university. I could even share the lab material, once it is in a reasonable state.
What files of the XPS / SDK projects do you think are useful? And where can I post it? Here?
Juergen
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-26-2012 07:07 AM
Juergen,
Please post on the forum.
You can use the "Attachments" option in the "Post Message" form to include a zip file.
Regards,
Mario.
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
01-27-2012 09:33 AM
Hi Mario
I attach an example IVK design for EDK 13.3. The design is based on the Camera_Frame_Buffer_Demo with an additional 2D-FIR block.
The zip contains the XPS and SDK projects. I removed the IVK_Repository for size reasons. This directory must be added at the top-level in order for XPS and SDK projects to compile.
Regards,
Juergen
Re: Porting PLB-based IVK Design to ISE 13.3
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
07-04-2012 12:39 PM
Juergen,
I found the issue with the fmc_iic_xps_IicRead routine.
I updated the code based on a more recent version of the xiic_low_level_dynamic_eeprom_example.c example from Xilinx.
In summary, the issue was caused by the fifth parameter to the XIic_DynSend( ) function call.
By changing this parameter from XIIC_REPEATED_START to XIIC_STOP, the issue was resolved.
int fmc_iic_xps_IicRead(fmc_iic_t *pIIC, Xuint8 ChipAddress, Xuint8 RegAddress,
Xuint8 *pBuffer, Xuint8 ByteCount)
{
Xuint8 ReceivedByteCount = 0;
Xuint8 SentByteCount = 0;
Xuint8 StatusReg;
XStatus TestStatus=XST_FAILURE;
int cnt = 0;
fmc_iic_xps_t *pContext = (fmc_iic_xps_t *)(pIIC->pContext);
// Position the Read pointer to specific location.
do
{
StatusReg = XIic_ReadReg(pContext->CoreAddress, XIIC_SR_REG_OFFSET);
if(!(StatusReg & XIIC_SR_BUS_BUSY_MASK))
{
SentByteCount = XIic_DynSend(pContext->CoreAddress, ChipAddress, (Xuint8 *)&RegAddress, 1,
XIIC_STOP);
}
cnt++;
} while(SentByteCount != 1 && (cnt < 100));
// Error writing chip address so return SentByteCount
if (SentByteCount < 1) { return SentByteCount; }
// Receive the data.
ReceivedByteCount = XIic_DynRecv(pContext->CoreAddress, ChipAddress, pBuffer, ByteCount);
// Return the number of bytes received.
return ReceivedByteCount;
}
The new fmc_iic_sw_2_02_a driver can be found in the 14.1 version of the camera design in the following forum post:
http://community.em.avnet.com/t5/Spartan-6-Industr
Regards,
Mario.