Reply
Topic Options
- Subscribe to RSS Feed
- Mark Topic as New
- Mark Topic as Read
- Float this Topic to the Top
- Bookmark
- Subscribe
- Printer Friendly Page
0
SRAM option for the S6LX16 Kit
Options
- Mark as New
- Bookmark
- Subscribe
- Subscribe to RSS Feed
- Highlight
- Email to a Friend
- Report Inappropriate Content
11-17-2010 12:48 PM
For those of you that would prefer to prototype with SRAM rather than LPDDR, Avnet has a compatible SRAM module that plugs onto the MXP (J1) header. You can find this module at
It includes a 1 MB (1 M x 8) MicroPower Cypress SRAM.
Cypress CY62158EV30LL-45ZSXI (http://www.cypress.com/?mpn=CY62158EV30LL-45ZSXI)
⎯ 1M x 8 organization
⎯ Very high speed: 45 ns
⎯ 3.3V operation
⎯ Ultra low standby power
o Typical standby current: 2 μA
o Maximum standby current: 8 μA
⎯ Ultra low active power
o Typical active current: 1.8 mA @ f = 1 MHz
⎯ Automatic power down when deselected
⎯ CMOS for optimum speed/power
⎯ Pb-free 44-pin TSOP II package
Bryan