Avnet Electronics Marketing - Community Forum
    |   
 
Home Design Services My Account About Avnet
Reply
Regular Visitor
TiagoPereira
Posts: 7
Registered: ‎10-06-2011
0
Accepted Solution

ML605 Led Testing by Hardware Co-Simulation

To whom it may concern,

 

I recently bought a ML605 kit from AVNET and I'm trying make a simple LED test controlled by the switches.

I get no errors performing a JTAG compilation or configuring the board, but the board(leds) don't light up in any way.

 

I attached my file hoping someone can help

 

Cheers,

 

Tiago

Avnet Employee
KountryK
Posts: 46
Registered: ‎07-09-2009
0

Re: ML605 Led Testing by Hardware Co-Simulation

Xilinx provides a large supply of reference designs that can be used on the ML605 board.  You can access these reference design with the following links.

http://www.xilinx.com/products/boards/ml605/reference_designs.htm

http://www.xilinx.com/products/boards/v6embd/reference_designs.htm

 

The "ML605 Built-In Self Test Applications" enable you to test out many features of the board, including the pushbutton switches & LEDs you are interested in.

 

Russ

Regular Visitor
TiagoPereira
Posts: 7
Registered: ‎10-06-2011
0

Re: ML605 Led Testing by Hardware Co-Simulation

[ Edited ]

Hi Kountryk,

 

I have access to both designs.

 

But not a single focus on mapping ports through Hardware Co-Simulation which is my current problem.

My BIST works fine by the way :smileywink:

Avnet Employee
brownman
Posts: 53
Registered: ‎07-07-2009
0

Re: ML605 Led Testing by Hardware Co-Simulation

Mapping of FPGA IO pins for HW co-simulation is not a topic covered by the ML605 User's Guide or reference designs.

 

I recommend reading Chapter 3 Using Hardware Co-simulation in the System Generator User Guide, especially the section titled Board Specific I/O Ports.